Part Number: RM46L852
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hi, all:
use RM46L852 microcontroller to generate a period wave for controlling a buzzer.
period: 2 seconds
duty: 10%
The pin is number 32 which named [MIBSPI5NCS[0]/EPWM4A] .
Using HALCOGEN, I selected EPWM4A in pinmux, enabled [Enable TBCLK sync] in [Special Pin Muxing] tab,
Enabled ETPWM drivers,
the next step:
but, I can't get the desired wave. BUZZER is always ringing, not period with 2 seconds.
any help is appreciated.
Best Regards
Daimb