Part Number: TM4C129CNCPDT
Other Parts Discussed in Thread: EK-TM4C129EXL
Tool/software: TI C/C++ Compiler
Hello Gurus,
I am trying to implement UART0 RX interrupt and can not implement yet. The code compiles successfully without any error. However I am facing two weird problems i.e;
- It doesnt capture any interrupt till I send the 8th character. As it receives the 8th character it services the interrupt handler ISR and returns back sucessfully
- It services the interrupt only once and never interrupts again no matter how many charter I send.
I have registered the interrupt handler in startup_css.c file already and declared as well.
//***************************************************************************** // // External declarations for the interrupt handlers used by the application. // //***************************************************************************** extern void xPortPendSVHandler(void); extern void vPortSVCHandler(void); extern void xPortSysTickHandler(void); extern void UART0ISR(void); //*****************************************************************************
AND
IntDefaultHandler, // GPIO Port B
IntDefaultHandler, // GPIO Port C
IntDefaultHandler, // GPIO Port D
IntDefaultHandler, // GPIO Port E
UART0ISR, // UART0 Rx and Tx
IntDefaultHandler, // UART1 Rx and Tx
IntDefaultHandler, // SSI0 Rx and Tx
IntDefaultHandler, // I2C0 Master and Slave
My main.c;
#include <stdint.h>
#include <stdbool.h>
#include "main.h"
#include "drivers/pinout.h"
#include "utils/uartstdio.h"
// TivaWare includes
#include "driverlib/sysctl.h"
#include "driverlib/debug.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/gpio.h"
#include "inc/hw_memmap.h"
#include "driverlib/pin_map.h"
#include "driverlib/uart.h"
#include "inc/hw_ints.h"
#include "driverlib/interrupt.h"
// FreeRTOS includes
#include "FreeRTOSConfig.h"
#include "FreeRTOS.h"
#include "task.h"
#include "queue.h"
// Tasks declarations
void LED1Task(void *pvParameters);
void LED2Task(void *pvParameters);
void LED3Task(void *pvParameters);
void LED4Task(void *pvParameters);
void SerialTask1(void *pvParameters);
void SerialTask2(void *pvParameters);
void UART0ISR(void);
// Main function
int main(void)
{
// Initialize system clock to 120 MHz
uint32_t output_clock_rate_hz;
output_clock_rate_hz = ROM_SysCtlClockFreqSet(
(SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480),
SYSTEM_CLOCK);
ASSERT(output_clock_rate_hz == SYSTEM_CLOCK);
// Initialize the GPIO pins for the Launchpad
PinoutSet(false, false);
// Set up the UART which is connected to the virtual COM port
//UARTStdioInit(0);
//UARTStdioConfig(0, 115200, SYSTEM_CLOCK);
/////////////////////////////////////////////////////////////////////////////
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//UARTConfigSetExpClk(UART0_BASE, output_clock_rate_hz, 115200,(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
UARTIntEnable(UART0_BASE, UART_INT_RX); //only enable RX interrupts
//IntRegister(INT_UART0, UART0ISR);
IntEnable(INT_UART0); //enable the UART interrupt
IntMasterEnable(); //enable processor interrupts
UARTStdioConfig(0, 115200, SYSTEM_CLOCK);
////////////////////////////////////////////////////////////////////////////
// Create demo tasks
xTaskCreate(LED1Task, (const portCHAR *)"LED1",
configMINIMAL_STACK_SIZE, NULL, 1, NULL);
//xTaskCreate(demoLED2Task, (const portCHAR *)"LED2",
//configMINIMAL_STACK_SIZE, NULL, 1, NULL);
xTaskCreate(LED3Task, (const portCHAR *)"LED3",
configMINIMAL_STACK_SIZE, NULL, 1, NULL);
//xTaskCreate(LED4Task, (const portCHAR *)"LED4",
//configMINIMAL_STACK_SIZE, NULL, 1, NULL);
xTaskCreate(SerialTask1, (const portCHAR *)"SerialTask1",
configMINIMAL_STACK_SIZE, NULL, 1, NULL);
xTaskCreate(SerialTask2, (const portCHAR *)"SerialTask2",
configMINIMAL_STACK_SIZE, NULL, 1, NULL);
vTaskStartScheduler();
/// Scheduler should NEVER reach here///
while(1)
{
//UARTprintf("Scheduler Error..!\n\r");
GPIOPinWrite(CLP_D1_PORT, CLP_D1_PIN, CLP_D1_PIN);
GPIOPinWrite(CLP_D2_PORT, CLP_D2_PIN, CLP_D2_PIN);
GPIOPinWrite(CLP_D3_PORT, CLP_D3_PIN, CLP_D3_PIN);
GPIOPinWrite(CLP_D4_PORT, CLP_D4_PIN, CLP_D4_PIN);
return 0;
}
}
and the UART0 handler defination;
void UART0ISR(void)
{
UARTIntClear(UART0_BASE, UART_INT_RX);
UARTprintf("UART0ISR called..!\n\r");
}
I am stuck and not able to identify the issue.
Any help/hint will be appreciable.
Thank you all.