Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hi,
so i have this code which from the times i executed it seems to do what i entended for it to do from the first place: ''entering Hibernate mode and then waking up with external push button''.
i'm suppose to make sure that my board did actualy enter hibernate mode and then woke up.
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// The interrupt handler for the Buttons.
//
//*****************************************************************************
void BottonsHandler(void){
if((GPIOIntStatus(GPIO_PORTF_BASE,true)& Buttoninit1))
{
GPIOIntClear(GPIO_PORTF_BASE,Buttoninit1);// Clear interrupt flag
TimerEnable(TIMER0_BASE, TIMER_A);//Enables the timer
}
else if((GPIOIntStatus(GPIO_PORTF_BASE,true)& Buttoninit0))
{
GPIOIntClear(GPIO_PORTF_BASE,Buttoninit0);// Clear interrupt flag
TimerDisable(TIMER0_BASE, TIMER_A);//Disables the timer
SysCtlPeripheralDisable(SYSCTL_PERIPH_HIBERNATE);//Disables the Hibernation module
HibernateGPIORetentionDisable();//Disable GPIO retention
HibernateDisable();//Disables the Hibernation module for operation.
}
}
void configureButtons(void){
//configureButton0
GPIOPinTypeGPIOInput(ButtonBase, Button0);
GPIOPadConfigSet(ButtonBase ,Button0,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);// Register our handler function for port F
GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_0,GPIO_FALLING_EDGE);// Configure PF4 for falling edge trigger
GPIOIntRegister(GPIO_PORTF_BASE,BottonsHandler); // Register our handler function for port F
GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_0);// Enable interrupt for PF0
//configureButton1
GPIOPinTypeGPIOInput(ButtonBase, Button1);
GPIOPadConfigSet(ButtonBase ,Button1,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);// Register our handler function for port F
GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_4,GPIO_FALLING_EDGE);// Configure PF4 for falling edge trigger
GPIOIntRegister(GPIO_PORTF_BASE,BottonsHandler);// Register our handler function for port F
GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_4);// Enable interrupt for PF4
}
void
Timer0IntHandler(void)
{
//
// Clear the timer interrupt.
//
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
UARTprintf("Hibernate mode is on!\n");
SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);// enable the hibernation module
HibernateEnableExpClk(SysCtlClockGet());//defines the clock supplied to the hibernation module
HibernateGPIORetentionEnable(); //Calling this function enables the GPIO pin state to be maintained during hibernation .
SysCtlDelay(SysCtlClockGet()/10 );
HibernateWakeSet(HIBERNATE_WAKE_PIN);//set the wake condition to the wake pin
SysCtlDelay(SysCtlClockGet()/10 );
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0);//turn off the green LED before the device goes to sleep.
/*enable the device to wake on either the RTC or the WAKE
pin. */
//HibernateRTCSet(0);
//HibernateRTCEnable();
// HibernateRTCMatchSet(0,10);
//HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC);
/*function requests the Hibernation module to disable the external regulator, removing power from the
processor and all peripherals.*/
HibernateRequest();
}
//*****************************************************************************
//
// Print "Hello World!" to the UART on the evaluation board.
//
//*****************************************************************************
int
main(void)
{
//volatile uint32_t ui32Loop;
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
//ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable the GPIO pins for the LED (PF2 & PF3).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
//
// Enable processor interrupts.
//
ROM_IntMasterEnable();
//
// Configure the two 32-bit periodic timers.
//
ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, ROM_SysCtlClockGet());
//
// Setup the interrupts for the timer timeouts.
//
ROM_IntEnable(INT_TIMER0A);
ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
//
// Registers an interrupt handler for the timer interrupt.
//
TimerIntRegister(TIMER0_BASE,TIMER_A,Timer0IntHandler);
//
// Initialize the UART.
//
ConfigureUART();
//
//Initialize the Buttons.
//
configureButtons();
//
// Hello!
//
UARTprintf("Hello, world!\n");
SysCtlDelay(SysCtlClockGet());
while(1)
{
UARTprintf("Run mode is on!\n");
SysCtlDelay(SysCtlClockGet());
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3,GPIO_PIN_3 );
SysCtlDelay(SysCtlClockGet()/10 );
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3,0);
SysCtlDelay(SysCtlClockGet()/10 );
}
}
i don't know how to proceed...any help !!
regards
amine