Part Number: TMS470MF06607
Other Parts Discussed in Thread: HALCOGEN
hi sir,
i am using the TMS470mf06607 microcontroller. with CCS V6.1.0.
i am using the SPI communication in my application .
i enabled the SPI base driver for transmit the data. i want to know how to receive the the data in to my buffer.
in the Halcogen code generator i enabled the TX interrupt also. in notification file also i did tha changes.
i copied my code in the below. can you please tell me how can receive the data from my slave device.
1) i want to transmit and receive the data. but i dont know how to receive the data.
i tried that receive function also. ( uint32 spiGetData(spiBASE_t *spi, uint32 group, uint16 * data); )
but i am not sure what i did it is correct or not.
2) i want to know how to toggle the chip select also.
any one please suggest me what are the changes i want to do in my program.
program:
#include "spi.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
uint32_t TG3_IS_Complete;
uint16 TG0_TX_DATA[8] = {0x1000, 0x1111, 0x1222, 0x1333, 0x1444, 0x1555, 0x1666, 0x1777};
uint16 TG0_RX_DATA[8]= {0};
uint16 TG1_TX_DATA[8] = {0x2000, 0x2111, 0x2222, 0x2333, 0x2444, 0x2555, 0x2666, 0x2777};
uint16 TG1_RX_DATA[8]= {0};
uint16 TG2_TX_DATA[8] = {0x3000, 0x3111, 0x3222, 0x3333, 0x3444, 0x3555, 0x3666, 0x3777};
uint16 TG2_RX_DATA[8]= {0};
uint16 TG3_TX_DATA[8] = {0x4000, 0x4111, 0x4222, 0x4333, 0x4444, 0x4555, 0x4666, 0x4777};
uint16 TG3_RX_DATA[8]= {0};
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
/* Enable CPU Interrupt through CPSR */
_enable_IRQ();
/* Initialize SPI Module Based on GUI configuration
* SPI1 - Master ( SIMO, SOMI, CLK, CS0 ) * */
spiInit();
/* Enable TG 0, 1, 2, 3 complete interrupt to INT 0 */
spiEnableGroupNotification(spiREG1,0,0);
spiEnableGroupNotification(spiREG1,1,0);
spiEnableGroupNotification(spiREG1,2,0);
spiEnableGroupNotification(spiREG1,3,0);
/* Fill the transfer Groups */
spiSetData(spiREG1,0,TG0_TX_DATA);
spiSetData(spiREG1,1,TG1_TX_DATA);
spiSetData(spiREG1,2,TG2_TX_DATA);
spiSetData(spiREG1,3,TG3_TX_DATA);
/* Enable TG0 to start, once tickCNT triggers */
while(1)
{
spiTransfer(spiREG1,0);
}
}
regards
Arun Kumar.N