Part Number: EK-TM4C1294XL
Hi Folks,
I wanted to build a distributed network based on RS485 bus communication with 9 bit UART configuration. I have 1 dedicated master, and 5 slave nodes in range of addresses between 1 to 5. To do this, I have implemented a modbus stack, where all of the slaves are waiting for the "9_bit_interrupt" and its subsequent bytes.
As I understood from the data sheet, if I set the address mask to 0xFF, the UART listen only its address. This works fine.
Then I tried to set an address mask to the first complement of the address, that caused that every slaves got every messages on the bus, which is not what I wanted.
Can anybody explain me, how can I use this address mask, how can I configure address ranges, etc?
Regards,
Norbert