Part Number: TM4C123GH6PM
Hello everyone,
I am using Tiva TM4C123GH6PM workshop workbook which I have attached below.Currently I am doing PWM Module experiment to drive Servo motor which is on page no. 321 of the workshop workbook.
In this program as it is mentioned in the manual, 83 is the center position to create a 1.5mS pulse from the PWM.Here’s how we came up with 83 … In the servo control code (covered shortly) we’re going to divide the PWM period by 1000. Since the programmed frequency is 55HZ and the period is 18.2mS, dividing that by 1000 gives us a pulse resolution of 1.82μS. Multiplying that by 83 gives us a pulse-width of 1.51mS. Other selections for the resolution, etc.would be just as valid as long as they produced a 1.5mS pulse-width. Take care though to be sure that your numbers will fit within the 16-bit registers.
Question 1.Why in the formula PWM Period is divided by 1000?
Question 2.Can we take any other Center frequency?
Question 3.What is meant by pulse resolution in this case?
Question 4.In the program ui8Adjust variable is taken which is in between 56 and 111.Is that mean motor will rotate in between 56 and 111 degrees or something else?
4762.TM4C123G_LaunchPad_Workshop_Workbook.pdf
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/debug.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "inc/hw_gpio.h"
#include "driverlib/rom.h"
#define PWM_FREQUENCY 55
int main(void)
{
volatile uint32_t ui32Load;
volatile uint32_t ui32PWMClock;
volatile uint8_t ui8Adjust;
ui8Adjust = 83;
ROM_SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
ROM_GPIOPinConfigure(GPIO_PD0_M1PWM0);
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
ui32PWMClock = SysCtlClockGet() / 64;
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, ui32Load);
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
ROM_PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT, true);
ROM_PWMGenEnable(PWM1_BASE, PWM_GEN_0);
while(1)
{
if(ROM_GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_4)==0x00)
{
ui8Adjust--;
if (ui8Adjust < 56)
{
ui8Adjust = 56;
}
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
}
if(ROM_GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_0)==0x00)
{
ui8Adjust++;
if (ui8Adjust > 111)
{
ui8Adjust = 111;
}
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Load / 1000);
}
ROM_SysCtlDelay(100000);
}
}