Part Number: TM4C1294NCPDT
Team,
my customer uses TM4C1294NCPDT in a new project. In order to reconfigure config values, the need to reprogram a small amount of flash during runtime. Config data is read and put into RAM where it is modified. Afterwards, the data is written back to flash.
They want to use the interrupt based flash programming routines as polling takes too long, but they sometimes get a fault as if they would access flash memory that is currently being programmed (fault ISR). Polling mode works fine.
Do you have any suggestion or example that demonstartes interrupt based flash programming?
Please let me know if you need more information.
Thanks!