Part Number: TM4C129ENCPDT
Does the D+ and D- polarity matter for USB communications? I ask because we built a custom board and now discovered these two traces are reversed. PL6 is connected to D- and PL7 is connected to D+.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C129ENCPDT
Does the D+ and D- polarity matter for USB communications? I ask because we built a custom board and now discovered these two traces are reversed. PL6 is connected to D- and PL7 is connected to D+.
My friend - Why would you risk this? Even if "this batch" of MCUs (may) work - or appear to work - there is NO Guarantee that "different lots" will behave in the identical manner.
The fact that such "polarity markings" are, "so well & repeatedly listed" - suggests rather strongly that, "Compliance is preferred & directed!"
We have gone ahead and performed the surgery on the board. The D+ and D- signals are now routed correctly to the USB connector, and miraculously, the usb_host_msc test we modified for our board is working.
The funny thing is that several people stared at the board, datasheet, TM4C129 design guidelines, TivaWare USB library documentation, the TivaWare example program, the software we modified for our board, etc., etc., and our eyes were so glazed over that we didn't notice the simplest thing -- the wires were crossed. Don't you just love those simple errors that escape detection?
Thanks to cb1 and Ralph Jacobi for your help.
You are FAR from alone in such staring - even as a group - especially as a group - and then "missing" an item of importance. This proves so (as we learned in the Army) due to the human eye first noting motion - then brightness - contrast - color... When the target field is static - attention notably drops off. And - when the "n+1" viewer arrives - knowing there have been "n" earlier views - n+1's "focus" is unlikely to "sustain & almost never peak."
So - can anything be done - to remedy such an issue? Certain board houses - for a fee - have advanced, automated means to verify your net-lists. We've witnessed both, "Traveling test pins, and very fine pitch fixed ones", both able to "far exceed" any "human board inspector." There are also "optical means" to scan boards - yet these "top out" @ 2-sided boards.
Any newly designed board proves an "adventure." If (any) volume is contemplated - engaging a board house w/proper, "Net-List" verification capability - makes great sense...
Most always - any/all "ICpins or connection points" - bearing such "polarity markings" - deserve increased scrutiny - even at the "schematic level" - especially at the "schematic level!" (as you well note - any error here is certain to propagate into the pcb!) Our firm demands a minimum of TWO to review - and agree/(sign off on) - the schematic's execution.
it would appear that such "polarity emphasis" was not recognized - or that the schematic review was (simply) faulty - for any number of reasons.
You wrote also of the board house, "catching build quality" (solder bridge, bad via, etc.) It has been my experience that this proves, "Not the case" - ONLY unassembled (naked) pcbs are so tested. The "flying/travelling" (expensive) test probes are (almost) certain to be damaged - when invited to engage a "populated board" - again "this proves outside" - firm's/my experience.
Indeed there ARE "Bed of Nails" methods - which "Can and Do" accommodate assembled boards - but these differ from the "Bare Pcb Test" (performed by the board vendor) as earlier described!
twelve12pm said:GND and VCC, well if you mix those up you'll notice right away! :-)
So true - and I am (still) "Living Proof of that!" Under intense client time-pressure - I made rapid changes to our motor-driver pcb - and then, "REVERSED the Power Inlet Polarity!" (normally our connector scheme prevents this - under "rush" I "bypassed!")
The (once) Filtering Electrolytics "signaled their displeasure" ... ... when the smoke (somewhat cleared) and "hearing restored" - it was agreed that (too often) "Haste makes Waste!"