This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GE6PM: TivaWare examples

Part Number: TM4C123GE6PM

Can TivaWare board level examples be modified to develop code? Specifically, can the Kentec display drivers such as kentec320X240X16ssd2119_8bit.c and kentec320X240X16ssd2119_8bit.h files be utilized? I know TivaWare is royalty free but can that modified example be used in a small applications. In the current Tivaware release these files are in the following directory :TivaWare_C_Series-2.1.4.178\examples\boards\ek-tm4c123gxl-boostxl-kentec-s1\drivers.

Thanks