Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: TM4C1230C3PM
We are recompiling driverlib.
We imported the driverlib project and told CCS to copy the project to our workspace. As expected, the resulting project references all source files as links to their original install location. Running a clean build appears to work, as it runs to completion and creates driverlib.lib with only one (expected) warning that the project was created using an older version of the compiler (5.2.6 [ARM], whereas we have 16.9.4 LTS). So it builds, but needs testing to make sure that our build environment, toolchain version, etc., did not introduce problems.
To that end, I have some specific questions:
I noticed that the driverlib CCS project sets the device to Tiva TM4C1230C3PM (see screenshot). Is there any particular reason why driverlib specifies TM4C1230C3PM? Does the choice of part have any effect on the resulting driverlib.lib binary? What prevents the library binary from having the wrong constants "burned in" if our application is destined for a different TM4C12x part?
Has anyone else recompiled driverlib, and are there any other gotchas we should look out for?
Thanks