Part Number: TMS570LC4357
Hello,
My Problem: I get no interrupts if a rising edge occurs.
I have generated a PWM-signal on pin 4 (2.5 kHz) and have configured pin 30 as an edge counter via HET IDE:
L00 CNT { reg=A,max=374,data=0};
L01 MCMP {en_pin_action=ON, pin=4, order=REG_GE_DATA, action= PULSELO, reg=A, data=0xBB, hr_data=0x40}
L02 ECNT { next = L00 , pin=30 , event = RISE , reg= B, irq=ON , data =0}
Pin 4 and Pin 30 are connected.
I have successfully measured the PWM-signal and have printed the value of the edge counter in a while loop, which increments.
I have configured Edge0 in HCG as follows:
My main-function:
int main(void)
{
/* USER CODE BEGIN (3) */
volatile uint32 EdgeCounter=0;
//_enable_IRQ();
hetInit();
edgeEnableNotification(hetREG1, edge0);
while(1){
EdgeCounter=edgeGetCounter(hetRAM1, 0);
printf("Edges:%d\n",EdgeCounter);
};
/* USER CODE END */
return 0;
}
I set breakpoints in the edgeNotification- and hetNotification-functions, but my program never lands there.
Did i forget something to configure in HCG?
Best regards
Kenan