Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hello,
Is it possible to measure the frequency on multiple HET pins without using the HR share setting?
I'd like to measure the frequency on HET1 pins 14,15,16, 21 and 22 (fixed by an existing hardware design). However, using the HALCoGen tool, I'm only able to measure frequency on one of the two pins in a HR share pair. For example, I can measure the frequency on either HET1 pin 14 or pin 15 depending on how I set the corresponding HR share bit, but not both at the same time.
Many thanks