This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: MibSPI inter-micro communication synchronization

Part Number: RM48L952

Hi,

I'm working on the communication bus the we implemented between two RM48.

A micro X is master and sends data to micro Y, which is slave, using MibSPI with a layout very similar to the one shown in your application note SPNA231 (High Speed Serial Bus Using the MibSPIP Module on Hercules):

  • X use to communicate MibSPI1, Y expect data on MibSPI3, the communication is uni-directional. SOMI is functional but pin is not effectively connected from Y to X (I don't care about data from Y) 
  • ENA and CS are functional to SPI (like in SPNA231)
  • I use on both side the full buffering size (128) (in SPNA231 on slave side the size is different)
  • On both side data transfer are managed by DMA: one control packet on X for SRAM>>DMA>>MIBSPI and two control packet on Y for MIBSPI>>DMA>>SRAM (like in SPNA231)

It works well but I'm need to make it more reliable about synchronization: my worry is that X doesn't know if slave have treated the received data. The data are in SRAM thank to DMA but if slave doesn't move DMA destination pointer or move the data, the master could start another transmission overwriting data. 

I thought I could use ENA to synchronize even frame transfer. It would work if slave disables its MibSPI transfer group after the transfer. I tried this by manually disabling the group and it works, slave doesn't move ENA and master goes to ENA time out, no data overwrite happens.

Here comes my questions,

  • considering that I've set "one shot transfer" in trasfer group configuration, why slave doesn't disable automatically the group after one transfer? 
  • do you see a better solution to synchronize the communication? As an alternative I've tried with DMACTRL bit "Auto-disable of DMA channel", effectively after the first transfer the transfer mibSPI>>SRAM doesn't happen but slave continues to give its ENA and master side is not notified.

Thanks!!!

PS: To come to a working solution I needed to learn on this forum about undocumented behavior of slave MibSPI (CS encoding, CSHOLD, ...). I pray to update the official TRM to include a section for slave MibSPI, these errata and lacks have been known for years and TRM of RM48 is 4 years old. If only my certification authority knew that my safety critical application is developed leveraging on undocumented features....

PPS: I really want to thank you for the precious and patient assistance you give on this forum

  • Hello Valerio,

    If you are using a similar methodology as described in the application note where you are completing the DMA transfers on blocks of data as they come in, the one shot may not be performing as expected because the TG never truly gets filled because you are moving data out almost as fast as it is coming in. This, in effect, is double buffering the incoming data.

    Some ideas to try instead of transferring data in small blocks as it comes in would be to setup the TG as a one shot mode and to trigger an interrupt when full, process the data from the TG storing results in RAM, then only re-enable the TG after data is processed. This may lose some efficiency but would allow you to continue to use the TG in one shot and eliminate the use of the DMA.

    A second option would be to continue as you are but, instead of allowing the MibSPI logic to control the nENA pin, set it up as a GIO and manually hold off the master until processing is done by manually manipulating the nENA pin as a GPIO.

    A third option would be to forego using a TG at all in the slave. i.e., set it up as a standard SPI receiving one byte at a time. Each byte received would then be transferred to the RAM buffer and, when full, commence processing before triggering the next DMA transfer of the next received data byte in the SPI Rx Buffer. Holding off the read of the Rx buffer would cause the ENA to hold off the master until the slave could read the received byte.

    And one final option, create another buffer for data that is being recieved. i.e., have a buffer one and a buffer two. When buffer one if being processed, buffer 2 can be in the process of being filled and vice versa. This would require the reconfiguration of the DMA transfers after the full receipt of each buffer.
  • Well, it seems that I have a lot attempts to implement ;-)
    I'll be back with my results.

    Thanks Chuck!
  • 1. “If you are using a similar methodology”

    Yes the methodology is similar with double DMA transfer, but I have a transfer group of 128 buffers and I transfer data to SRAM with two DMA transfer, each applied on 64 buffers.

    2. “the one shot may not be performing as expected because the TG never truly gets filled”

    This does not seem true. I tried to completely disable DMA transfer but the TG does not get disabled anyway. I see that the 128 MibSPI buffers are filled with new data from master (overwriting the old one) but the TG is still active. In fact if I send again data from the master I find new data again in slave buffers. I'm not able in any way to automatically disable the TG on slave side. What am I missing?

     3. Your idea 1 (Eliminate the use of DMA and transfer data from MibSPI buffers with CPU, re-enable the TG after data is processed)

    Also giving up with DMA (which is something I would like to avoid), currently it doesn’t work for me because of the problem in point 2

     4. Your idea 2 (nENA pin set up as a GIO)

    This doesn’t seem to fit my needs, if I understood well. If I manually enable the transfer, I cannot guarantee that the slave is fast enough to manually disable the ENA and avoid the second transfer.

    Anyway this opens another strange phenomenon: if on the slave side ENA is set as GIO and DMA transfer is enabled, one or two data word get lost. The slave receives well the first 64 buffers which triggers the first DMA block transfer, after that the second or third data are never received, in this way the second block of 64 buffers never gets filled, as a result slave become desynchronized. It seems like that if a MibSPI is under DMA transfer is somehow busy and lose incoming data. This does not happen if I set ENA as functional or I disable DMA transfer. Can you find any reason for this?

    5. Your idea 3 (forego using a TG, set it up as a standard SPI)

    This seems an option but I would like to leverage on the big relaxing of time requirement that MibSPI buffers give.

    6. Your final option (create another buffer)

    If I understood right what you are saying, it is more or less what I’m currently doing. I have 64 buffers which trigger a DMA transfer and another 64 buffers which trigger another DMA transfer. But again this does not guarantee synchronization with master.

    So if you have any suggestion on point 2 I would like to give it another try, otherwise I will choose another way following your ideas unfortunately renouncing to some of mibSPI capabilities.

    Thank you for your attention,

    Valerio

  • Hello Valerio,

    Have you been able to resolve this issue or is there still the ongoing issue?
  • Hi Chuck,
    unfortunately not in the way I wanted. Since no answer came from TI and TRM documentation is lacking about MibSPI topic, I'm trying another way.

    My solution is similar to the one described in https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/158061/1978463.

    I'm using DMA chain to get a circular buffer: one DMA channel transfers data and the other (in chain) transfers a counter into a variable. Reading that variable I know how many frames DMA has transferred.

    This works but I don't like:

    • nothing automatically stops the transfers, there is the possibility to overflow the buffer overwriting old data. As you read in my previous posts, this is something I'd tried to managed through MibSPI (oneshot tranfer + ENA)
    • though this approach is used by other people on the forum, It seems to me like a little undocumented hack

    So currently I think I will go this way managing the occurrence of buffer overflow along all the dataflow. This is delayed by MibSPI buffers and DMA circular buffer, but still possible.

    Valerio