Part Number: TMS570LC4357
Other Parts Discussed in Thread: TPS65381A-Q1
Hello everyone,
I recently assembled an own board with the TMS570LC4357, I now know that I made some mistakes (written below) and my boards are not operational. For the next boards I want to be sure that all layout design errors are gone but for that I would like to know what error is being reported by the ESM.
The schematics/layout errors that I have noticed are:
VCCP is not powered at all, should be powered by 1.2V
VCCF is powered by 1.2 and should be powered by 3.3V
I can access the icepick tap, but no further tap (no dap either), is there a way to access other TAPS or to the ESM registers to know what error is being reported?
I am using the TPS65381A-Q1 to power the MCU
Greetings
Antonio