Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/RM48L952: Frtos HEAP on RM48L952 SDRAM

Part Number: RM48L952

Tool/software: TI-RTOS

Hi,

I'm trying to use an external SDRAM for allocate 8 MB of HEAP (Full size is 16MB, other 8MB is for my RAMDisk), as my product will be storing big data on the RAM, so I need to allocate a lot of memory.

My SDRAM is already tested and should work correctly and my RAMDisk with FRTOS FAT16 as well.

This thread has almost the same problem but no solution:    e2e.ti.com/.../371084

I tried many things to place the RTOS Heap into the SRDAM, but it always ended in a abort after prvSetupDefaultMPU(); or vPortStartFirstTask(); in "os_port.c "

I tried it with the "os_heap.c" and with "heap_5.c" .

I also expanded the MPU settings in prvSetupDefaultMPU(); with

prvMpuSetRegion(portPRIVILEGED_RAM_REGION,  0x80000000, portMPU_SIZE_16MB | portMPU_REGION_ENABLE, portMPU_PRIV_RW_USER_RW_EXEC | portMPU_NORMAL_OIWTNOWA_SHARED);

but it also ended with an abort after prvSetupDefaultMPU();

Is it possible to put the heap on the SDRAM or is there still a problem with the HW like in the thread above?

Thanks.