Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Hello,
As I mentioned above I am using Hercules TMS570LS1227 Microcontroller and would like to use the eCAP module to capture a signal generated by a Hall Effect Sensor.
I previously used the eCAP etPWM example included in HALCoGen and it worked successfully, then I used the function generator to generate a PWM and the eCAP module successfully captured it. However, when I tried to capture the PWM signal coming from the Hall Effect Sensor, the eCAP module couldn't capture it.
I am currently using VCLK4 frequency at 80 MHz and no prescale settings.
The example in HALCoGen works with frequency ranges of 200 KHz thru 5 MHz.
I need to measure the frequency of a much more slower signal coming from the Hall Effect Sensor that ranges between 1 Hz and 208 Hz. Is there a way to set up the eCAP to measure very slow frequencies?
Thanks,
Jesus Galindo