Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: TM4C1294NCPDT, ADS127L01,
Tool/software: Code Composer Studio
Sup Y'all
I'm using this launchpad for a mixed signal project. I'm running up against an issue where I really need high speeds and good resolution so I can measure activity in the 250kHz range. I'm considering marrying my launchpad with this MCP3911 (https://www.mouser.com/ds/2/268/20002286C-1150165.pdf) which goes up to ~4MHz but I'm not keen on writing my own SPI drivers for this. I'm wondering if anyone in the community has driver code for a fast external ADC ~+2MHz...
I figure since TI probably makes quite a few ADC's that'll meet that spec, this problem's probably solved already. If anyone could help me out I'd appreciate it greatly
Cheers,
Jim