Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, UNIFLASH,
Hi Hercules Team,
I have a customer trying to fix the below error:
An error occurred while trying to generate source files from HALCoGen. Please ensure that the model has been configured correctly: 'HALCOGEN' is not recognized as an internal or external command, operable program or batch file
When loading CAN examples from "C:\ti\Hercules\HALCoGen\v04.07.00\examples "
Below is the error the customer has, when trying to load a Simulink compiled file using UniFlash:
"Error!
File "x/first5.out" Does not match the target endianness, not loaded. Check project build options and target configuration file (ccxml)."
We think that issues may be related to firmware the customer loaded on the TMS570LC43x launch pad when using CCS7 and HALCoGen 4.07. With the Mathworks embedded coder, they're using CCS6 and HALCoGen 4.06, which we think may require an older version of firmware on TMS570LC43x launch pad.
The customer has tried using HALCoGen 04.07 and 04.06, having issues with both, see below.
Would you please be able to help locate correct version of firmware for TMS570LC43x launch pad, and possibly be provide instructions on downgrading firmware, as well as verifying this as a fix?
Thanks in advance!
Barend