Part Number: TMS570LC4357
Hi,
I am using a TMS570LC4357 package ZWT and I want to use MIBSPI2NCS[1] (pin D3 only).
I configured the output multiplexing register PINMMR35[13] as indicated in table 4-28 in the datasheet / table 6-1 in the TRM.
But I was confused then as I found the same pin configurable also for input multiplexing in table 6-2 of the TRM.
In the Reference manual, table 6-2 indicates that MIBSPI2NCS[1] is available on D3 pin if PINMMR88[17] = 1.
In the Datasheet, table 4-29, the MIBSPI2NCS[1] is not listed in the same table.
My questions are:
- Which input pin multiplexing table is applicable?
- if the table from the TRM is applicable, then do I need to configure the PINMMR88 if I use this pin for SPI communication, and why? Would the answer be different if I was using the MIBSPI2NCS[1] pin as a GPIO input? GPIO output?
Best regards,
Gael