This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: errata EMIF#5

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Hello,

We are currently using your following component: TMS570LC4357.

By using HalcoGen, we are seeing a comment about EMIF usage restriction.

Indeed, it is mentioned : "As per the errata EMIF#5, EMIF SDRAM initialization must performed with EMIF clock below 40MHz."

Is this Erratum applicable also for TMS570LC4357 device ?

here is an extract from HalcoGen:

"

** @fn void emif_SDRAMInit(void)
*   @brief Initializes the emif Driver for SDRAM
*
*   This function has been deprecated.
*   As per the errata EMIF#5, EMIF SDRAM initialization must performed with EMIF clock below 40MHz.
*   Hence the init function needs to be called from the startup before the PLL is configured.
*   A new function emif_SDRAM_StartupInit has been added and is called from the startup.
*   This function need not be called from the main, and is preserved for compatibilty.
*/

void emif_SDRAMInit(void)

"

Best regards,

Christopher