Part Number: TMS570LS1114
Dear Experts:
I am working on TMS570LS11x && TMS570LS12x Bootloader .Now I make sure the PC Side Code work well and I transplant the code in my own Hyper Terminal which is designed based on VS2010. I still have some questions to verify my Bootloader function.
My device is TMS570LS1114 for example and the hardware platform is my own board which designed by ourselves.
Now I have correctly generated a file whose form is Prj_DCAN_Test.bin. But why I find My PC cast lots of time more than 60 secends to load data? I find the Image(APP bin file) only 29K.
In fact, My program is still stop in the same position.
Can I add a breakpoint after the next instruction to verify my bootloader receiving the data?
Now I will display the main modify section to you,Please give me some advice to solve the interface problem.
The Code is
#1 bl_config.h
#define CAN_BIT 500000 /*can be 125K, 250K, 500K, 750K, 1000K. The default is 125K*/
#define SYS_CLK_FREQ 160 //MHz
#2 flash_defines.h
#define TMS570LS11
#3 bl_dcan.c
g_ulForced =1 ;
Due to my hardware platform which is lack of a test pin PORTA 7 ,So I forcedly
Updaata by change the flag valve.
After operate the above steps.I see the Memory Broser 0x00010000 ,and I find no data?
Whether I invalidly operate ?
Best and Regards
Qiuchi