Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software: Code Composer Studio
Hi,
I have custom design board with TM4C1294NCPDT with USB device port. We are planning to use it as serial debug port. When I power on this board, the USB serial port doesn't show up on Windows (Win7). I suspect the USB pin assignment may has some problem. The example application of EK-TM4C1294XL initialized PB0-1/PD6/PL6-7 are used for USB. But in my code (ported from example code, USB_device_cserial) I just initialized PL6-7 because PB0-1 are used for other purpose. I notice that the datasheet of this device mentioned (on page 1769):
"... If the USB controller is used as either a dedicated Host or Device, the
DEVMOD field in the USB General-Purpose Control and Status (USBGPCS) register can
be used to connect the USB0VBUS and/or USB0ID inputs to fixed levels internally, freeing
the PB0 and PB1 pins for GPIO use. "
My question is, if I need PB0-1 for other purpose, how should I initial the USB with only using PL6-7? the VBUS and ID pins are no connected in my design.
thanks,