Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
Hi Friends,
Iam working on ek-tm4c1294xl kit ,currently iam trying to integrate adc with udma iam attaching .iam having that it unable to tranfer data from buffer to destination .In this program iam trying print the data that i have captured in adc.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "utils/cpu_usage.h"
#include "utils/uartstdio.h"
#include "utils/ustdlib.h"
#include "utils/uartstdio.c"
#include "driverlib/adc.h"
#include "inc/hw_adc.h"
static int i;
#define MEM_BUFFER_SIZE 1024
#define UART_TXBUF_SIZE 256
#define UART_RXBUF_SIZE 256
//static uint32_t g_ui8TxBuf[UART_TXBUF_SIZE];
static uint32_t g_ui8RxBufA[UART_RXBUF_SIZE];
static uint32_t g_ui8RxBufB[UART_RXBUF_SIZE];
static uint32_t g_ui32uDMAErrCount = 0;
static uint32_t g_ui32BadISR = 0;
static uint32_t g_ui32RxBufACount = 0;
static uint32_t g_ui32RxBufBCount = 0;
uint32_t g_ui32SysClock;
#if defined(ewarm)
#pragma data_alignment=1024
uint8_t pui8ControlTable[1024];
#elif defined(ccs)
#pragma DATA_ALIGN(pui8ControlTable, 1024)
uint8_t pui8ControlTable[1024];
#else
uint8_t pui8ControlTable[1024] __attribute__ ((aligned(1024)));
#endif
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
ui32Status = uDMAErrorStatusGet();
if(ui32Status)
{
uDMAErrorStatusClear();
g_ui32uDMAErrCount++;
}
}
void ADCseq0Handler()
{
uint_fast16_t ui16Idx;
uint32_t ui32Status;
uint32_t ui32Mode;
for(ui16Idx = 0; ui16Idx < UART_TXBUF_SIZE; ui16Idx++)
{
UARTprintf("printing forom receiver side");
UARTprintf("hello receiver %d",g_ui8RxBufA[ui16Idx] );
}
ADCIntClearEx(ADC0_BASE, ADC_INT_DMA_SS0 | ADC_INT_SS0);
if (uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT) == UDMA_MODE_STOP) {
// found the full buffer
// re-set up a DMA transfer to the buffer
uDMAChannelTransferSet((UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT), UDMA_MODE_PINGPONG, (void *)(ADC0_BASE + ADC_O_SSFIFO0), g_ui8RxBufA, sizeof(g_ui8RxBufA));
}
if (uDMAChannelModeGet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT) == UDMA_MODE_STOP) {
// found the full buffer
// re-set up a DMA transfer to the buffer
uDMAChannelTransferSet((UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT), UDMA_MODE_PINGPONG, (void *)(ADC0_BASE + ADC_O_SSFIFO0), g_ui8RxBufB, sizeof(g_ui8RxBufB));
}
/* if(!uDMAChannelIsEnabled(UDMA_CHANNEL_ADC0))
{
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ui8TxBuf,
(void *)( ADC0_BASE + ADC_O_SSFIFO0),
sizeof(g_ui8TxBuf));
uDMAChannelEnable(UDMA_CHANNEL_ADC0);
}*/
}
void
InitUART1Transfer(void)
{
uint32_t div;
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_ADC0);
ADCClockConfigSet(ADC0_BASE,ADC_CLOCK_SRC_PLL,ADC_CLOCK_RATE_FULL);
ADCSequenceConfigure(ADC0_BASE, 0 /*SS0*/, ADC_TRIGGER_ALWAYS, 3 /*priority*/); // SS0-SS3 priorities must always be different
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 0, ADC_CTL_TS); // ADC_CTL_TS = read temp sensor
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 1, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 2, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 3, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 4, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 5, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 6, ADC_CTL_TS);
ADCSequenceStepConfigure(ADC0_BASE, 0 /*SS0*/, 7, ADC_CTL_TS | ADC_CTL_END | ADC_CTL_IE); // ADC_CTL_IE fires every 8 samples
ADCSequenceEnable(ADC0_BASE, 0);
ADCSequenceDMAEnable(ADC0_BASE, 0);
uDMAChannelAttributeDisable(UDMA_CHANNEL_ADC0,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
uDMAChannelControlSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_NONE | UDMA_DST_INC_8 |
UDMA_ARB_4);
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
g_ui8RxBufA, sizeof(g_ui8RxBufA));
uDMAChannelTransferSet(UDMA_CHANNEL_ADC0 | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(void *)(ADC0_BASE + ADC_O_SSFIFO0),
g_ui8RxBufB, sizeof(g_ui8RxBufB));
uDMAChannelEnable(UDMA_CHANNEL_ADC0);
ADCIntEnableEx(ADC0_BASE, ADC_INT_DMA_SS0);
IntEnable(INT_ADC0SS0);
}
void
ConfigureUART(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART0);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 115200, g_ui32SysClock);
}
int
main(void)
{
static uint32_t ui32PrevUARTCount = 0;
uint32_t ui32XfersCompleted;
uint32_t ui32BytesTransferred;
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
SysCtlPeripheralClockGating(true);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
ConfigureUART();
UARTprintf("Tiva C Series @ %u MHz\n\n", g_ui32SysClock / 1000000);
UARTprintf("CPU\tRemaining\tMemory\t\t\t UART\n");
UARTprintf("Usage\tTime\t\tTransfers\t\t Transfers\n");
SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
IntEnable(INT_UDMAERR);
uDMAEnable();
uDMAControlBaseSet(pui8ControlTable);
InitUART1Transfer();
SysCtlSleep();
UARTprintf("\nStopped\n");
IntDisable(INT_ADC0SS0);
IntDisable(INT_UDMA);
}