Part Number: RM57L843
Hi
I need to use MibSPI as a normal SPI with SPI Flash. Two questions,
1)- I'm using MibSPI as a normal SPI using only one CS and floating all other CS. Rest of the connections are straightforward like the normal SPI using MOSI, SIMO and Clk with slave device. Please confirm this hardware configuration is enough and nothing special required in H/W to use it in SPI mode.
2)- I consider that it will not impact DMA and I can use DMA mode in the SPI to avoid extra load on CPU. What is maximum length data offer in DMA for an SPI. Please confirm?
Regards;