Part Number: TM4C1294NCPDT
Tool/software: TI C/C++ Compiler
Hi
(a) I was wondering if there way for TM4C to generate jitter-able clock output to keep EMI low, for example, +/-5% variation on say 300KHz or 1MHz (for SEPIC PSU).
(b) I'm going to use 16MHz XTAL into TM4C and boost system clock to around 100MHz or so (it early stage). I like to add small jitter again to keep EMI low. Bear in mind the USB will be connected to embedded Window 10 module. What the best way to do this?
Thank in advance for your consideration.