Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: Programming the TM4C1294ncpdti directly avoiding the debug micro

Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA

I have the eval board which is to be the basis of a board I'm developing. I will be using CCS (or Energia) for code development and have been programming the device using the USB lead connected to my laptop and programming direct through CCS (or Energia).

I now want to remove the debug micro from the process so that the eval board mimics my final hardware for programming purposes.

I presume i connect via the external debug connection using a JTAG programmer? Can you tell me which programmer i need to obtain and any modifications i need to make to the debug board (jumpers etc) for this to work.

Thanks.