Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1227: TMS570LS1227 zero-dominant

Part Number: TMS570LS1227

In TMS570LS1227 16- and 32-Bit RISC Flash Microcontroller's datasheet have the below description :

 

but,how to understand "zero-dominant".

  • Hello,

    Meaning of zero-dominant output buffers:
    If two outputs are shorted together and one of them is driving a 1 while the other is driving a 0, then the result will be a 0 if the output buffers driving both the outputs are "zero-dominant" output buffers.