Part Number: TMDXRM57LHDK
Tool/software: Code Composer Studio
Hello,
I am working on a project that receives and processes a rather large amount of Sensor Data (2k Byte every 60ms). I have found and implemented the Example Code for SCI DMA successfully. So the problem I have is not with the actual receiving of Data, but rather with Notifications.
Ideally I would want to be notified once with every fully received package, so once every ~60ms. Right now I am using a Function that is called periodically every 1-2ms (with every µC Cycle) and should return true if a new Package is received and false in between. With my current Implementation it allways returns true. The Code is as follows:
bool DMATransfer()
{
if(dmaGetInterruptStatus(DMA_CH1, LFS))
{
// Restart
sciREG4->CLEARINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
dmaSetChEnable(DMA_CH1, DMA_HW);
sciREG4->SETINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
return true;
}
return false;
}
I would greatly appreciate any advice to solve this problem.
Regards,
Lars