Part Number: SW-EK-TM4C1294XL
Other Parts Discussed in Thread: EK-TM4C1294XL
Hello,
I am trying to establish a UART connection between the two above boards. I am making a connection between the RX and TX of the UART pins on the SMARTRF0EB (not the USB port - the pins are located at the bottom -right of the board) and the UART0 and UART1 of the EK-TM4C1294XL. I am using the example codes for UART for both boards but I get no data on the EK-TM4C1294XL.
On the EK-TM4C1294XL I am using TIRTOS.
Can someone please explain the procedure for both the right way to connect these two boards as well as the code required for a UART connection to be done. When debugging I see that the ports are being opened successfully . I will post my codes on a later post.
Thanks,
Vikram