Part Number: TMS570LS3137
There is some confusion regarding the MibSPI max baud rate for the TMS570LS3137. The tech reference manual states a maximum baud rate of 20MHz.
See spnu499b section 25.1:
The data sheet specifies a minimum cycle time of the SPI clock pin as 40ns (which equates to a 25MHz baud rate).
See spns162 section 5.10.4:
Also we are currently configuring MibSPI 1 to run at 26.667 MHz and it appears to be working (see attached scope plot).
What is the actual maximum baud rate of the MibSPI on the TMS570LS3137? Can we expect any issues running above the 20MHz specified in the technical reference manual?