This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301: Hercules TMS570SL1227 Control Card: Motor doesn't spin

Part Number: DRV8301
Other Parts Discussed in Thread: MOTORWARE

Hi there

I am using a TMS570SL1227 Control Card and a DRV8301 Kit; SW is CCS v7.4 and MotorWare Software Projects for Hercules Safety MCU's v1.00.03.03.

I followed all the instructions from DRV8301-LS12-KIT_README_FIRST.pdf as well as foc_encoder_speed_ls12.pdf.

I am able to compile and download, but afterwards the software expects a command (in sys_main.c):

// Endless loop to wait for start command from either GUI or button
    while(DRV_get_Enable(drvHandle) != 1){
        if(GetChar(drv.ecmpHandle) == '2')
        {
               gGUIObj.EnableFlg=1;
               PutText(drv.ecmpHandle, "Motor Enabled\r\n");
        }
        GUI_run((GUI_Handle)&gGUIObj, drvHandle, graphHandle);
    }

I commented this line out and disbabled all SCI passages, but the motor doens't spin, when I set “gGUIObj.EnableFlg” = 1" and “gGUIObj.calibrateEnable = 1". 

Is the software/hardware out of date? Is there a newer/better option available (motor control on hercules)?