Part Number: TM4C123GH6PGE
Hello.

EK_TM4C123GXL to DK-TM4C123G migration and modify
Why can not I write "Hello :)" in the Err1.txt file?
Please let me know what to do.
regards.
static int printFileStructure (void) {
uint32_t ui32ItemCount;
FRESULT fresult;
static char *pcBuf;//[256]="Hello World";
uint32_t ui32BytesWritten;
//
// Open the file by name that was determined above. If the file exists
// it will be opened, and if not it will be created.
//
fresult = f_open(&g_sFileObject, "Err1.txt", (FA_CREATE_NEW |FA_WRITE));
if(fresult != FR_OK)
{
*(&pcBuf) ="Hello:)";
f_write(&g_sFileObject, &pcBuf, 20, (UINT *)&ui32BytesWritten);
return(0);
}
*(&pcBuf)="Hello:)";
fresult = f_write(&g_sFileObject, &pcBuf, 20, (UINT *)&ui32BytesWritten);
//
// Open the current directory for access.
//
fresult = f_opendir(&g_sDirObject, g_cCwdBuf);
f_write reference location
- TivaWare_C_Series-2.1.4.178\third_party\fatfs\doc\en
create File in USB
- Attach capture