Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: AMC7820
Tool/software: Code Composer Studio
Hi,
In my design I have to configure 2 slave modules in SPI2.
The slave module i used is TI- AMC7820.
First i tried to configure single SPI module.
The Pins I used was PD0,PD1 and PD3. The chip select was PK3 for slave 1.
I have modified the code for write 0x2345 to a register and read back it. But what I read back is NULL
The init,read and write functions are as below.
void SSI2Init(void) //SPI 2 initialization
{
//
// The SSI2 peripheral must be enabled for use.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);// CS1 K3
//
// Configure the pin muxing for SSI0 functions on port D0, D1, and D3.
//
GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);
GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
GPIOPinConfigure(GPIO_PD3_SSI2CLK);
// GPIOPinConfigure(GPIO_PA3_SSI0FSS);// This is not done as CS is a GPIO pin
GPIOPinTypeGPIOOutput(GPIO_PORTK_BASE, GPIO_PIN_3);// CS1 for slave 1 as GPIO output pin
GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_3,GPIO_PIN_3);//make it high, as it is active low
//
// Configure the GPIO settings for the SSI pins.
//
GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_3 | GPIO_PIN_1 | GPIO_PIN_0);
//
// Configure and enable the SSI port for SPI master mode. Use SSI2,
//
SSIConfigSetExpClk(SSI2_BASE, g_ui32SysClock, SSI_FRF_TI,
SSI_MODE_MASTER, 1000000, 8);
//
// Enable the SSI2 module.
//
SSIEnable(SSI2_BASE);
//
// Read any residual data from the SSI port.
//
while(SSIDataGetNonBlocking(SSI2_BASE, &pui32DataRx[0]))
{
}
}
void SPI2Read(void)
{
pui32DataTx[0]=0x82;// for reading from register
pui32DataTx[1]=0x40;
GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_3 ,0);// CS LOw; AMC expects Active low control signal
for(ui32Index = 0; ui32Index < 2; ui32Index++)
{
//
// Send the data using the "blocking" put function. This function
// will wait until there is room in the send FIFO before returning.
// This allows you to assure that all the data you send makes it into
// the send FIFO.
//
SSIDataPut(SSI2_BASE, pui32DataTx[ui32Index]);
}
//
// Wait until SSI0 is done transferring all the data in the transmit FIFO.
//
while(SSIBusy(SSI2_BASE))
{
}
// Receive 2 bytes of data.
//
for(ui32Index = 0; ui32Index < 2; ui32Index++)
{
//
// Receive the data using the "blocking" Get function. This function
// will wait until there is data in the receive FIFO before returning.
//
SSIDataGet(SPIBase, &pui32DataRx[ui32Index]);
// Since we are using 8-bit data, mask off the MSB.
//
pui32DataRx[ui32Index] &= 0x00FF;
}
GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_3 ,GPIO_PIN_3 );// Reset CS to High
}
void SPIwrite(void)
{
pui32DataTx[0]=0x02;
pui32DataTx[1]=0x40;
pui32DataTx[2]=0x23;
pui32DataTx[3]=0x45;
GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_3 ,0)// CS LOw; AMC expects Active low control signal
for(ui32Index = 0; ui32Index < 4; ui32Index++)
{
//
// Send the data using the "blocking" put function. This function
// will wait until there is room in the send FIFO before returning.
// This allows you to assure that all the data you send makes it into
// the send FIFO.
//
SSIDataPut(SSI2_BASE, pui32DataTx[ui32Index]);
}
//
// Wait until SSI0 is done transferring all the data in the transmit FIFO.
//
while(SSIBusy(SSI2_BASE))
{
}
GPIOPinWrite(GPIO_PORTK_BASE, GPIO_PIN_3 ,GPIO_PIN_3 );// Reset CS to High
}
Please Help me.
Thanks in advance.