Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: HALCOGEN
Good day. I wanted to use temperature sensors.
I used appnote and example code for settup of the temp sensors. It is available at this link: http://www.ti.com/lit/an/spna216/spna216.pdf
I even downloaded a zip-archive with this example
(it just didnt work when i opened it in CCS, so i decided to create new Halcogen project and make everything the same)
But when i laucn the code i get the "ErrorCode = 1".
Code goes here and that's all. It cannot calibrate the sensors. Where can be the problem?
Here is the example project.8484.temperatura.zip