Greetings Community.
I need help to develop a control system project.
I was assigned a project that involves the development of a PID for a propeller motor to maintain the angular position of a pivoted bar using the wind force of the propeller. The project requires the implementation of a TM4C123GXL using the Code Composer Studio C language to create the PID. The angular position sensor must be an accelerometer and a gyroscope module, such as the MPU6050.
Unfortunately, I was not provided with an adequate introduction or a course of the Code Composer Studio software for the development of my project.
I'm at zero. If someone can guide me on how to star, I will be really grateful.
Here's an example of the control system.