Part Number: TMS570LS1224
Hello Team,
We have below set of questions on NERROR pin:
1) Can the NERROR pin be configured as Open drain??
2) What is use of General Purpose Register (GPREG1) (bit[13] controls signal nERROR) ?? What is low EMI output buffer mode??
3) NERROR in Datasheet is mentioned as I/O. Can it be configured as input?? If yes what is usecase?
4) Datasheet says NERROR has 8 ma drive capability. What does it mean?? Is it Limited to 8 mA or it is the minimum guarnteed value?