Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C1294XL, TM4C1294NCPDT, , TM4C129XNCZAD
Tool/software: Code Composer Studio
Wth the help of CMSIS DSP library i was running one of the example code "arm_fft_bin_example_f32.c".
THIS IS THE CODE:
#include "arm_math.h"
#include "arm_const_structs.h"
#define TEST_LENGTH_SAMPLES 2048
/* -------------------------------------------------------------------
* External Input and Output buffer Declarations for FFT Bin Example
* ------------------------------------------------------------------- */
extern float32_t testInput_f32_10khz[TEST_LENGTH_SAMPLES];
static float32_t testOutput[TEST_LENGTH_SAMPLES/2];
/* ------------------------------------------------------------------
* Global variables for FFT Bin Example
* ------------------------------------------------------------------- */
uint32_t fftSize = 1024;
uint32_t ifftFlag = 0;
uint32_t doBitReverse = 1;
/* Reference index at which max energy of bin ocuurs */
uint32_t refIndex = 213, testIndex = 0;
/* ----------------------------------------------------------------------
* Max magnitude FFT Bin test
* ------------------------------------------------------------------- */
int32_t main(void)
{
arm_status status;
float32_t maxValue;
status = ARM_MATH_SUCCESS;
/* Process the data through the CFFT/CIFFT module */
arm_cfft_f32(&arm_cfft_sR_f32_len1024, testInput_f32_10khz, ifftFlag, doBitReverse);
/* Process the data through the Complex Magnitude Module for
calculating the magnitude at each bin */
arm_cmplx_mag_f32(testInput_f32_10khz, testOutput, fftSize);
/* Calculates maxValue and returns corresponding BIN value */
arm_max_f32(testOutput, fftSize, &maxValue, &testIndex);
if (testIndex != refIndex)
{
status = ARM_MATH_TEST_FAILURE;
}
/* ----------------------------------------------------------------------
** Loop here if the signals fail the PASS check.
** This denotes a test failure
** ------------------------------------------------------------------- */
if ( status != ARM_MATH_SUCCESS)
{
while (1);
}
while (1); /* main function does not return */
}
AFTER BUILDING THE CODE THIS IS THE ERROR COMING:
SO WHAT IS THIS ERROR WHY IS IT COMING?