Part Number: TMS570LS1114
Hello,
Could you tell me how to set the ACK filed bytes in the DCAN? I want to know which rigister?
Best and Regard
Qiuchi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1114
Hello,
Could you tell me how to set the ACK filed bytes in the DCAN? I want to know which rigister?
Best and Regard
Qiuchi
The ACK FIELD is two bits long and contains the ACK SLOT and the ACK DELIMITER. In the ACK FIELD the transmitting station sends two ’recessive’ bits. A RECEIVER which has received a valid message correctly, reports this to the TRANSMITTER by sending a ’dominant’ bit during the ACK SLOT (it sends ’ACK’).
Dear QJ Wang:
There are still some issue bothering me about ACK bit.
From the Spnu515b, I do not sure if RxOK bit and TxOK is the ACK bit. So, I test the two bits.
Watch Expression display the value of “ES_TxOK_flag=0 “and “ES_RxOK_flag=0”.
I still have trouble to watch the bit. Is the picture from the spnu515b?Sorry for my poor knowledge.
Thanks and Regards
Qiuchi
Dear QJ Wang
I wanna watch the TX/RX state,but still have not found the ACK bit in this datasheet”spnu515b”.Could you tell me where to find ACK register bit in the attachment named "spnu515b"? It is better to know which page in this datasheet. I do not know how to watch it from CAN Bus.
Not: the attachment is the spnu515b.
Thanks and Regards
Qiuchi