Part Number: TM4C1290NCPDT
Hi,
I have to implement a crc16-ccitt as explained in http://srecord.sourceforge.net/crc16-ccitt.html#results
This says for the textstring "1234546789", I should get "0xEC55", which also is the expected value of my specification.
Although the code in the webpage works, I think it would be nice to make use of the CRC in the driverlib.
My Code here is
uint32_t uRes=0;
char zTest []="123456789";
MAP_CRCConfigSet(CCM0_BASE,
CRC_CFG_INIT_SEED |
CRC_CFG_TYPE_P1021 |
CRC_CFG_SIZE_8BIT);
CRCSeedSet(CCM0_BASE,0xFFFF);
uRes = CRCDataProcess(CCM0_BASE, zTest, 9,false );
As an result I get 0x29B1, which is said to be an "bad crc calculation" in the link, it says "Among the problems with the “Bad_CRC” implementation is that it does not augment a zero-length message with 16 zero bits, as is required (either implicitly or explicitly) when calculating the standard CRC. Thus, it reports a CRC of 0xFFFF — not 0x1D0F — for a zero-length message"
Any Ideas how to adapt to get the desired results are welcome.
Regards
Micky