Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Here is the code:
#include "arm_math.h"
#include "arm_const_structs.h"
#define TEST_LENGTH_SAMPLES 2048
/* -------------------------------------------------------------------
* External Input and Output buffer Declarations for FFT Bin Example
* ------------------------------------------------------------------- */
/* ------------------------------------------------------------------
* Global variables for FFT Bin Example
* ------------------------------------------------------------------- */
uint32_t fftSize = 1024;
uint32_t ifftFlag = 0;
uint32_t doBitReverse = 1;
/* Reference index at which max energy of bin ocuurs */
/* ----------------------------------------------------------------------
* Max magnitude FFT Bin test
* ------------------------------------------------------------------- */
int32_t main(void)
{
float32_t maxValue;
status = ARM_MATH_SUCCESS;
/* Process the data through the CFFT/CIFFT module */
/* Process the data through the Complex Magnitude Module for
calculating the magnitude at each bin */
/* Calculates maxValue and returns corresponding BIN value */
{
status = ARM_MATH_TEST_FAILURE;
}
/* ----------------------------------------------------------------------
** Loop here if the signals fail the PASS check.
** This denotes a test failure
** ------------------------------------------------------------------- */
if ( status != ARM_MATH_SUCCESS)
{
while (1);
}
while (1); /* main function does not return */
}