Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hi,
I have a question regarding self-tests and STC tests of the TMS570LS3137. I'm currently analyzing a piece of code which tests STCSCSCR[3:0] in the assembler startup code to decide if a reset caused by a STC test. If this is true, a jump is taken to continue with the STC test (after reset). However, I've now seen in spnu499b.pdf that STCSCSCR[3:0] is reset to it's default value on a CPU reset. Is this also true for a reset triggered by the STC test?
Best regards,
Michael