This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: EMAC0 is working perfectly on custom PCB

Guru 56418 points

Part Number: TM4C1294KCPDT

It remains unclear why so many posters end up in this forum with a custom PCB that EMAC0 fails.

Our custom PCB even has TX/RX traces both foil sides. However the length of each differential pair was made almost identical and VIA kept to even numbers and minimal. Also used 1uf caps versus 0.1uf following the recommendations for separate rail power traces feeding the Pulse XFMR. Many times rallied around that suggestion absent any response from several posters.

Following the TM4C129x System Design guidelines (SPMA056–October 2013) seems to have paid off....

Thank You TI engineers for going the mile on that document!