Part Number: TMS570LC4357
Hello everybody,
I am trying to setup a serial communication (SCI) and see the outcome on the terminal, unfortunately I have not been successful. I have two messages but I only see the one from the printf. I have tried with SCI1, 2,3 and 4 without any change. Here is my code:
#include <stdio.h>
#include "HL_sys_common.h"
#include "HL_sci.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define SCI_PORT sciREG2
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
uint32_t delay = 0;
sciInit();
while(1)
{
sciSend(SCI_PORT, 15, "Putty Terminal\n");
printf("CCS Terminal\n");
for (delay = 0; delay < 5000; delay++);
}
/* USER CODE END */
}
I forgot to say, I configured Halogen to use Baudrate of 9600 and Putty uses that baudrate, too. The same with parity bits, stop bits, etc.
Thank you in advance and kind regards,
JG