Part Number: TM4C1294NCPDT
1) Starting with TiVaware 2.14->Example->boards->ek-tm4c1294xl->enet_lwip, it uses DHCP option, and it works fine
2) Based on //e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/396803
3) lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP) is replaced with
struct ip_addr ipaddr, netmask, gw;
IP4_ADDR(&gw, 192,168,0,1);
IP4_ADDR(&ipaddr, 192,168,0,222);
IP4_ADDR(&netmask, 255,255,255,0);
lwIPInit(g_ui32SysClock, pui8MACArray, ipaddr.addr, netmask.addr , gw.addr , IPADDR_USE_STATIC); //192.168.0.222
The project compiles fine, but will not acquire the IP, did I miss something?