Part Number: TM4C1294NCPDT
Dear Master,
1. My customer wants to do the ethernet verification, does TI have the application to show the command list like an example below(it's from other vandor's application note)?
Initial Setting:
Write Reg. 31 Data = 0x0000 //page 0
Write Reg. 9 Data = 0x0000
Write Reg. 4 Data = 0x0061
*Write Reg. 25 Data = 0x0843 //10Mbps waveform without EEE
Write Reg. 0 Data = 0x9200 //PHY reset
*Note: For 10Mbps waveform test “with EEE”, please change this line to be:
Write Reg. 25 Data=0x0853
..................................
2. what's the recommended impedance(layout trace) should be between the RJ45 and ENTX / RX ?
thanks in advance