Part Number: LAUNCHXL2-570LC43
Good day, i have a following problem. I'm using EMIF SDRAM to store a data. When i write data to sdram every 1000ms for some time everything is fine. But sometimes data corruption occurs like this :
What can this be?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL2-570LC43
Good day, i have a following problem. I'm using EMIF SDRAM to store a data. When i write data to sdram every 1000ms for some time everything is fine. But sometimes data corruption occurs like this :
What can this be?
Hi Roman,
Do you mean that the written data and the readback data don't match? Please do another test:
1. disable cache: _cacheDisable_()
2. write a bunch of 32-bit words to SDRAM: I use the address as the data in my sample code
void WRITW32BIT_ADR(unsigned int Start_Address, unsigned int No_Of_Words){
unsigned int *Addr = (unsigned int *) Start_Address;
while(No_Of_Words > 0) {
*Addr++ = Start_Address++;
No_Of_Words--;
}
}
3. readback those data and check if they match each other
unsigned int CHECK_EMIF_MEMORY_32BIT_ADR( unsigned int Start_Address, unsigned int No_Of_Words)
{
unsigned int ReadPattern;
unsigned int *Addr = (unsigned int *) Start_Address;
while(No_Of_Words > 0)
{
ReadPattern = *Addr++;
if (ReadPattern != Start_Address)
{
return (Start_Address);
}
No_Of_Words--;
Start_Address++;
}
return (0);
}
This is SDRAM configuration used for the SDRAM on HDK (IS42S1640).:
void emif_SDRAM_StartupInit(void)
{
/* USER CODE BEGIN (11) */
/* USER CODE END */
volatile uint32 buffer;
/* Procedure B Step 1: EMIF Clock Frequency is assumed to be configured in the startup */
/* Procedure B Step 2: Program SDTIMR and SDSRETR to satisfy requirements of SDRAM Device */
emifREG->SDTIMR = (uint32)((uint32)2U << 27U)|
(uint32)((uint32)0U << 24U)|
(uint32)((uint32)0U << 23U)|
(uint32)((uint32)0U << 20U)|
(uint32)((uint32)0U << 19U)|
(uint32)((uint32)0U << 16U)|
(uint32)((uint32)1U << 12U)|
(uint32)((uint32)2U << 8U)|
(uint32)((uint32)0U << 7U)|
(uint32)((uint32)0U << 4U)|
(uint32)((uint32)0U << 3U);
emifREG->SDSRETR = (uint32)2U;
/* Procedure B Step 3: Program the RR Field of SDRCR to provide 200us of initialization time */
emifREG->SDRCR = 1605U;
/* Procedure B Step 4: Program SDRCR to Trigger Initialization Sequence */
/** -general clearing of register
* -for NM for setting 16 bit data bus
* -cas latency
* -BIT11_9CLOCK to allow the cl field to be written
* -selecting the banks
* -setting the pagesize
*/
emifREG->SDCR = (uint32)((uint32)0U << 31U)|
(uint32)((uint32)1U << 14U)|
(uint32)((uint32)2U << 9U)|
(uint32)((uint32)1U << 8U)|
(uint32)((uint32)2U << 4U)|
(uint32)((uint32)elements_256);
/* Procedure B Step 5: Read of SDRAM memory location causes processor to wait until SDRAM Initialization completes */
buffer = *PTR;
/* prevents optimization */
buffer = buffer;
/* Procedure B Step 6: Program the RR field to the default Refresh Interval of the SDRAM*/
emifREG->SDRCR = 585U;
/* Place the EMIF in Self Refresh Mode For Clock Change */
/* Must only write to the upper byte of the SDCR to avoid */
/* a second intiialization sequence */
/* The byte address depends on endian (0x3U in LE, 0x00 in BE32) */
*((unsigned char *)(&emifREG->SDCR) + 0x0U) = 0x80;
/* USER CODE BEGIN (12) */
/* USER CODE END */
}