Part Number: TM4C129XNCZAD
Hi,
I configured my TM4C129XNCZAD to run at 120MHz and trying to output this clock speed through PQ4. However, I am not able to get it even through the settings of the register are correct. The maximum frequency I can see is 60MHz. I am just wondering if this is the limit of the GPIO speed?