Part Number: TMS570LS0432
Other Parts Discussed in Thread: BQ76PL455A,
Tool/software: Code Composer Studio
Hello,
I'm trying to send a message from my TMS570LS0432 Launchpad to the bq76pl455a.
In the CCS Example code there are several lines where the variable "nSent"is used.
But i cant understand how it's send via the UART.
An example:
void main(void)
{
/* USER CODE BEGIN (3) */
systemInit();
gioInit();
sciInit();
sciSetBaudrate(scilinREG, BAUDRATE);
rtiInit();
vimInit();
_enable_IRQ();
WakePL455();
CommClear();
CommReset();
// initialize local variables
int nSent, nRead, nTopFound = 0;
int nDev_ID, nGrp_ID;
BYTE bFrame[132];
uint32 wTemp = 0;
/** Code examples
* The command sequences below are examples of the message examples in the bq76PL455 Communication Examples document.
* each message example references the section in the document.
*/
// Wake all devices
// The wake tone will awaken any device that is already in shutdown and the pwrdown will shutdown any device
// that is already awake. The least number of times to sequence wake and pwrdown will be half the number of
// boards to cover the worst case combination of boards already awake or shutdown.
for(nDev_ID = 0; nDev_ID < TOTALBOARDS>>1; nDev_ID++) {
nSent = WriteReg(nDev_ID, 12, 0x40, 1, FRMWRT_ALL_NR); // send out broadcast pwrdown command
delayms(5); //~5ms
WakePL455();
delayms(5); //~5ms
}
// Mask Customer Checksum Fault bit
nSent = WriteReg(0, 107, 0x8000, 2, FRMWRT_ALL_NR); // clear all fault summary flags
// Clear all faults
nSent = WriteReg(0, 82, 0xFFC0, 2, FRMWRT_ALL_NR); // clear all fault summary flags
nSent = WriteReg(0, 81, 0x38, 1, FRMWRT_ALL_NR); // clear fault flags in the system status register