Part Number: EK-TM4C123GXL
Tool/software: Linux
Hello All,
I am working on Audio Signal Processing project (Kind of Spectrum Analyzer) and for that I'm using Raspberry Pie 3 and TFT Display.
But as we know Raspberry Pie-3 don't have inbuilt ADC so I want to use ADC of TM4c123 and transfer data to RP-3.
Now my question is
1] Is it possible to connect TM4C123 and RP-3?
2] The analog Input signal specifications are 500mVpp/20KHz. (TM4C123 have 12bit ADC with reference voltage 3.3 Volts and sampling rate upto 1MHz)
Now after taking samples in TM4C123 how much speed I can achieve while transferring sampled data to RP-3?
3] Is it any other method to do sampling of Analog signal with sampling rate of around 200 KHz and give the digital samples to RP-3 at higher data rate?
Thanks,
Vinay Kumar