Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hi. We are using the Hercules RM48l952zwt. with 5.2.12 TI bootloader for the RM 48 and 4.3.00 HalCoGen.When there is an AC (power) brownout, a board the boots with HalCoGen generated init code is Ok. However, we ship with the TI bootloader that then loads the HalCogen code and our application.The Hercules board with the TI bootloader version on the board which does the minor board bring up then loads the rest of the halcogen software corrupts the flash on banks 1,2 and 7 if AC fluctuates (brownouts) during the bootloader running. What do we need to change in the TI bootloader initializing the board so it is as stable as the halcogen generated code initializing the board, and this does not happen? Thank you.